11/6/2024 12:50 PM | |
Joined: 11/2/2024 Last visit: 11/6/2024 Posts: 1 Rating: (0) |
I use: S7 1214 6ES7 214-1AG40-0XB0 Firmwire V 4.5.1 TiaPortal V16 Ethrnet\IP library V1.0.3 (for S7-1200) LCCF_EnetScaner I try to connect air island ESV-EP32 I installed the library, configured all the settings, In attachment photo DB & OB blocks and *.eds file. PLS, help AttachmentPictures.zip (3 Downloads) |
Last edited by: MacSim at: 11/06/2024 13:59:21 |
|
11/6/2024 2:32 PM | |
Joined: 8/12/2021 Last visit: 11/6/2024 Posts: 331 Rating: (30) |
Hi! You can find on the documentation the meaning of the error code. I would suggest you use a logic error to verify if si the state that you have to focus. Sometimes, communication problems begin with a status and then change. |
Last edited by: Moderator_Lan at: 11/06/2024 14:46:09Link optimized If this Information really helps, you could use the Rate function |
|
Follow us on