7/9/2021 10:18 AM | |
Posts: 1 Rating: (0) |
-My machine have 5 motor connect to 5 Inverter Micromster 440, (Name motor is M1, M2, M3,M4,M5) all motor control by the PC through profibus COM link. -When I run 5 motor so all motor run ok . -When I run only motor M4 so this motor run ok too -But when stop motor M4 and run 4 other motor ok , I get fault F0422 on Inverter of motor M4, why Inverter M4 get fault like that ? although Inverter M4 was Stop in this task. -Note : Inverter M4 is new one I just replace for old one, when I replace I was use AOP panel to copy all parameter from old one to new one. I has success some time with copy and paste parameter like that for other inverter but this time is fail . -Can you give me the way to delete this fault F0422. ------------------------------------------------------------------------------------------ |
Last edited by: Mr Two at: 07/09/2021 10:23:54Last edited by: Jen_Moderator at: 07/09/2021 11:54:00New subject after splitting |
|
Follow us on