12/16/2022 7:03 AM | |
Joined: 6/30/2014 Last visit: 8/4/2025 Posts: 475 Rating:
|
Hello Mayra, That scenario sounds like if there are two issues: - uninstalling COMOS and/y - error with code -2000 because of the license for COMOS. Now, if your intention is to use COMOS, I would not uninstall it but open a ticket at the Support: they surely know that error, they will help you to solve the issue about the COMOS license. Uninstalling COMOS will for sure not solve the error with code -2000. In order to speed up the solution, maybe you can send them a copy of the used/affected license file (is surely a XML file, never something else), also please list the steps you have done until now. After that, you can be successfull with it. In case of further questions, let us know here. With best wishes, SuperPippo |
Follow us on