12/21/2021 4:42 PM | |
Joined: 2/10/2020 Last visit: 5/21/2024 Posts: 3 Rating: (1) |
Hello, has anyone helped in this problem. I want to improve my block and have only one input in FB with HW_ID of device. Now in my block i have extension to 10 inputs with HwSubmodule constant in case when programmer want to maps all inputs from device which has a few input process images like COGNEX cam. This FB has additional diagnostic functions for the module/device from which inputs are read. Mr. 0_Einstein, in my opinion this is good solution which could make programmer life easier. We don't need create tags for modules or external devices in Profinet and we have one universal block to map all inputs to whatever DB using only one input info like HW_ID. Can be there anything easier? But how to read all inputs from module/device... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/22/2021 11:04:23New subject after splitting |
|
1/4/2022 11:29 AM | |
Joined: 1/24/2014 Last visit: 10/29/2024 Posts: 127 Rating: (6) |
Hi I am just studying the question, because I read here (1200) : That puzzles me. I believe that using DPRD_DAT increases the use of PN and cycle time, but significantly or not ? I'm waiting for the delivery to test all this...
I guess I will have to test both solutions and compare. |
Follow us on