10/10/2014 9:52 AM | |
Joined: 3/20/2012 Last visit: 4/26/2024 Posts: 118 Rating: (1) |
Hello The MAG3100 with MAG5000 suits at my needs. But they need to be in conformity with the "Arrêté du 19 décembre 2011 " (french laws!!!). This rule just asks that the systems has been certified par an organism that is itslef cerified by: - Comité français d'accréditation (COFRAC), - or by body signer of the international agreement " European Cooperation for Accreditation of Laboratories " ( EAL), So i've found an environment certificate here, produced by "SIRA / CSA group": http://support.automation.siemens.com/WW/view/en/33099337 For me it's all ok, but one cartificate is missing: i've got nothing to say that "SIRA / CSA group" is accreditate buy COFRAC or as signed the EAL. In fact, the French environment law just asks to use quality mesurement systems (accuracy better than 5%, easy!). Any idea? Best regards Olivier. |
10/10/2014 5:13 PM | |
Joined: 3/28/2010 Last visit: 5/20/2024 Posts: 1032 Rating: (211) |
Not my field, but if you check out the EC Declaration of Conformity, https://cache.automation.siemens.com/dnl/TM/TM1MDE3AAAA_69270816_Appr/A5E31813160A_003.pdf and go to page 4, at the bottom you'll find a French agency listed, SGS CTS, with an address. Call them and ask how to navigate the bureaucratic labryinth of French regulations. |
Follow us on