1/30/2025 8:48 AM | |
Joined: 8/22/2011 Last visit: 9/7/2025 Posts: 2 Rating:
|
Dear All, We have a task to make communication via Modbus TCP using Siemens S7-1200 CPU 1214C and Weintek cMT3102X HMI (Weintek is on another machine and the manufacturer predicted to communicate with other devices this way). Using a PC app for testing (ModbusDoctor) we retrieved the data successfully. However, we can not establish communication using PLC S7-1200. Every time we start communication, the status parameter is 7006 - Data is being received. But it stays there forever and the Error code is appearing every few seconds with 80C8 code - No response. In the attachment, we are sending images of a configuration of ModbusDoctor (working one), an image of the configuration of MB_Client and the TIA portal App that we tried. Our PLC address is 192.168.250.25 , Weintek HMI Address is 192.168.250.26 , PC, when we were using ModbusDOctor, was on IP 192.168.250.27. We tried to use the ethernet port on PLC and with CP 1243-1 but we had no success. Please, can some of the experts look at this and help us? Best regards, LoMi AttachmentDocumentsAndProgram.zip (153 Downloads) |
Last edited by: LoMi at: 01/30/2025 08:49:30Last edited by: LoMi at: 01/30/2025 08:56:26 |
|
Follow us on