11/20/2019 1:17 AM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (106) |
Hello Jorge KW, Inside SIMOCODE pro V operating manual Motor management and control devices
SIMOCODE ES 2007 Premium • Complete device parameterization • Online access through local device interface • Graphical editor • Extended monitoring and diagnostic functions • Convenience functions • Online access via PROFIBUS DP • Online access via remote access • STEP 7 integration So your answer is yes, you have to have on SCADA PC installed SIMOCODE ES 2007 Premium
Useful link Full manual , chapter 3 is the interesting one. Looks like Profinet is much more recommended option due to OPC UA and web server availability. Best Regards Soble |
Last edited by: SOble at: 11/20/2019 01:18:19Last edited by: SOble at: 11/20/2019 02:15:06Last edited by: SOble at: 11/20/2019 02:23:31Website: |
|
11/20/2019 10:07 AM | |
Posts: 80 Rating: (0) |
Thanks for your elaborate and very useful answer. This is what I expected, I have to integrate the SIMOCODE Premium SW in my TIA installation. I do not expect to use a PROFIBUS fiber connection for this though. My intention is to reach the components the next way: Development PC and SCADA -------- (Fiber) ------ SCALANCE XB205-3 -----(Profinet) --- S7-1500 -----(Profibus master card) ------ SIMOCODEs. I had concerns because of PROFINET to PROFIBUS conversion to reach the SIMOCODEs through routing. Would this be fine?
|
11/20/2019 1:47 PM | |
Posts: 80 Rating: (0) |
Helo SOble, According to this link it might be possible, wouldn't it? Isnt this a way to reach DP slaves via PROFINET? The only thing is that I do not have the Simatic PC Station or Simatic Manager. I only have TIA portal, is it now integrated in TIA portal?
|
Last edited by: Jen_Moderator at: 11/21/2019 07:21:45Optimized link. |
|
11/20/2019 3:26 PM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (106) |
Your CM and CPU are on the list, I cant post two files: and had to cut pics on previous post: Yes you can: open link and check two download links below: Take a look picture it is your example, and keep CPU as I/O controller Yes it would work in your case. |
Last edited by: SOble at: 11/20/2019 15:41:14Last edited by: Jen_Moderator at: 11/21/2019 07:22:31Optimized link. Website: |
|
11/20/2019 3:44 PM | |
Posts: 80 Rating: (0) |
Great then! Thanks very much Regards, Jorge |
This contribution was helpful to1 thankful Users |
Follow us on