2/6/2007 9:31 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello sfestiva, When you connect the TP to X1 port of CPU, you are connected through MPI ![]() Have you seen this link: about routing? http://support.automation.siemens.com/WW/view/en/11012204 Perhaps it's usefull Best regards, Wizard |
2/6/2007 9:37 AM | |
Joined: 1/30/2007 Last visit: 6/3/2022 Posts: 262 Rating:
|
Hello sfestiva, first i presume you connected the profibus to the S7-200 on x2 of the cpu. If you connect the TP270 on the same line (plug) you should see all 3 cpu. If there are any reasons to divide the line and to connect the TP270 only to the cpu314 you need to param. a 'routing'-connection in the hw-config through the cpu314. http://support.automation.siemens.com/WW/view/en/11012204 Cincerely |
Last edited by: Simaticus at: 2/6/2007 9:37 AM |
|
Follow us on