1/27/2015 9:53 AM | |
Posts: 18 Rating:
|
Dear all, I have a S7-400H system with two cp441-2 in slave mode, the master is given the data but in the slave the communication is really slow. I need to put a different slave number? Anyway I have a realy to change the wiring to one o another depence which one is the master. I read that is not possible to put a redudant cp 441-2 in the S7-400H system. Enclosed you can find the configuration of the system. Thanks in advance! --------------- New subject after splitting from S7-400H - CP441-2 - Redundant slave Modbus AttachmentConfiguration.zip (281 Downloads) |
Last edited by: Min_Moderator at: 1/27/2015 2:06 PMSplitted |
|
This contribution was helpful to
1 thankful Users |
Follow us on