9/18/2022 7:01 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Your screenshot is not helpful. Did you define the path under "Extras" in which you saved the UDF? |
9/20/2022 6:38 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
See attached screeenshot. I have no problem, but I have Win7 and LSC V7.1.5. |
9/20/2022 6:49 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
You can also see in your screenshot that the "Data Log Profile" directory with the "Data Log" block is missing. |
9/23/2022 1:44 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
But the LOGO! 0BA4 has not the function UDF. Only LOGO! 0BA7 and also LOGO! 0BA8. The LOGO! 0BA4 is a very, very old LOGO!, produced from the year 2003 to 2005. LOGO! ..0BA4 Released for DeliveryManufacture of LOGO! ..0BA4 to Be Discontinued (Type Discontinuation) |
Follow us on