9/20/2023 11:10 AM | |
Joined: 2/8/2016 Last visit: 2/29/2024 Posts: 1 Rating: (0) |
Cannot seem to resolve this fault. Fault occurs randomly once a day, but only for a brief moment, then reset fault, crane off and on and carry on with production. Hoist is always used when fault occurs, but sometime with hoist and trolley. Swapped out VSB & -G10 (24V power supply), tested IR, not sure about current drawn when fault occurs, but it never seem to exceed the max the AFE is set up for. Would like to swap out CUSA, but not sure of the procedure and possible complications. Some parameters in DriveMon shows "Code word missing", "Parameter deactivated" - not sure if that is normal or something wrong? Where are the CT's located for me to test them? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/21/2023 06:26:03New subject after splitting. Quote inserted. |
|
Follow us on