7/4/2024 6:30 PM | |
Joined: 4/6/2021 Last visit: 9/1/2024 Posts: 2 Rating: (0) |
Hi All, I have WinCC Unified V18 update 3 running and cannot get the autologin feature to work, followed the manual, this link, this other link but to no avail. It should be easy enough, just set the autologin feature in runtime manager with proper user name and password but even after several tries... I'm running the runtime manager in a windows server standard 2022 and the HMI is running on chrome under windows 10 IoT LTSC. |
7/22/2024 12:01 PM | |
Joined: 2/17/2020 Last visit: 9/17/2024 Posts: 1060 Rating: (192) |
Hi, I believe you could use this workaround to enable Automatic login on remote web clients: WinCC Unified V16: Auto login browser extension for google chrome So, if the clients work with Chrome, they could use this extension to log in automatically. |
A rating will be well appreciated. |
|
Follow us on