2/7/2012 8:55 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, It could be that the probelm is SP3 of Windows XP as Protool is not released for it. Information about the compatibility between the Windows operating systems and the ProTool versions can be found under entry-ID 8795248. Best regards, Hristo Mihalev |
2/7/2012 9:44 AM | |
Posts: 8 Rating:
|
Yes, I saw that sheet earlier. In other conversations, there has been problems with XP SP3, but not similar. I'm just curious, if any one has had same problem or has anyone been able to use Protool with XP SP3 properly. |
2/7/2012 12:11 PM | |
Posts: 3037 Rating:
|
Hello, Do youhavea PG M3 with a serial interface? If you use a converter from USB to serial, then the download to OP27does not work. Tweety |
2/8/2012 8:44 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
To be honest at the moment my PC (inbuilt serial port) has Protool installed on XP SP3 and I can transfer/upload without any problem. Also here in forum you can find a lot of members which complain about SP3 but on the same time a lot of members which confirmed properly working of Protool in SP3. Take a look at ProTool 6.0 SP 3 with Windows XP SP3. But if we come back to Field PG M3 - are you sure you have there serial port? Give its MLFB number. Best regards, Hristo Mihalev |
2/8/2012 12:50 PM | |
Posts: 8 Rating:
|
Hello, MLFB is 6ES7715-1BB20-0AA1 And error in Protool: E4020: Internal Error Download 00003621H No connction to the OP! Protool version 6 SP3 Best Regards Sakke |
2/8/2012 3:01 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Then you are also using a "mini adapter" Serial port adapter D9/D25 See also: http://support.automation.siemens.com/WW/view/en/17354655 Best regards, Wizard |
Follow us on