6/29/2022 11:14 AM | |
Joined: 3/11/2019 Last visit: 8/6/2024 Posts: 1545 Rating:
|
Hi Mirza, for migration, also a installation of STEP 7 classic (and all optional software packages used in classic project) are needed as a precondition. Only TIA for migration, is not enough. But you can also use trial version of STEP 7 classic for migration to TIA. But if you want to migrate another project after the trial period has ended, it will not be possible anymore. If you want to migrate a project to TIA, and classic is not installed on this system, you will receive an error message. You can use migration tool instead on an other system, but then classic also must be installed on the other system. What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?"The software components listed below must be installed on the computer on which you wish to perform the migration:
***EDIT*** The "combo" license includes STEP7 classic, so it is not necessary to buy a "combo" license and a sencond license for classic. regards sancruz |
Last edited by: sancruz at: 06/29/2022 11:28:53Last edited by: sancruz at: 06/29/2022 11:29:13Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
6/29/2022 1:01 PM | |
Joined: 11/18/2018 Last visit: 7/25/2024 Posts: 4 Rating:
|
Thank you Sir |
6/29/2022 1:02 PM | |
Joined: 11/18/2018 Last visit: 7/25/2024 Posts: 4 Rating:
|
Thank You sancruz, is clear now |
Follow us on