1/29/2009 9:58 AM | |
Posts: 43 Rating: (0) |
Dear all, i have task to change two motor drives of wound rotor type with new VFD drives, data about old drives is given in atachments, i need some sugestions which drives should be good for this application
Attachmentmotor data.pdf (331 Downloads) |
2/2/2009 12:24 PM | |
Posts: 43 Rating: (0) |
Sorry for my bed english, my task here is to change those old motors with new motors which will be controled by MM |
2/10/2009 10:25 AM | |
Posts: 43 Rating: (0) |
Thanks for reply, but i am not sure that i can produce starting moment on the output from the shaft of biger motor, because gear ratio from output shaft to smaller motor shaft is 476 andgear ratio from output shaft tobiger motor shaft is 97. in attachment i am sending schematics of gearbox.
Attachmentreduktor_small1.zip (210 Downloads) |
2/12/2009 8:28 AM | |
Posts: 43 Rating: (0) |
Hello Here is the picture, but quality is low because when i got better quality file size is 541KB and it can not be uploded, thanks for the replies Attachmentreduktor4.pdf (271 Downloads) |
Follow us on