5/24/2007 11:31 AM | |
Joined: 8/31/2005 Last visit: 7/18/2024 Posts: 2198 Rating: (328) |
Hello, It should work. (I didn't check the SW-versions, see the lower text.) Make shure to habe a PG/PC in your net-configuration, otherwise the routing will not work. See this FAQ, look at the configuration in Netpro. S7 Technology ( S7 T Config is part of it) includes Starter, the configuration Tool for MM, and Sinamics. Please note this FAQ.It shows on Page 6 which Starter version is included in S7 Technology. A MM4 firmware may need at least a Starter Version (MM4 Firmware Vx.y requires Starter Va.b or higher) But as far as I know, there are not so many FW-versions for MM as there are for SINAMICS. |
Last edited by: miami at: 24.05.2007 11:35 |
|
Follow us on