3/10/2023 12:19 PM | |
Joined: 3/9/2023 Last visit: 3/13/2023 Posts: 6 Rating: (0) |
Hello guys . one question please, i don't have a memory card in PLC 1500 . How can i creat a path inside the PLC but without memory card ? I'm trying to use te FILEWRITE, but i don't have the memory card to save the data. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: U_797ccdba-2e83-4a72-9b3d-1febb4b1af74 at: 03/10/2023 12:20:55Last edited by: Jen_Moderator at: 03/13/2023 06:40:24New subject after splitting |
|
3/10/2023 12:23 PM | |
Joined: 3/9/2023 Last visit: 3/13/2023 Posts: 6 Rating: (0) |
So if i want ro read and write the data and save it i need to have a memory card ? |
3/10/2023 12:24 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986) |
correct |
This contribution was helpful to1 thankful Users |
3/10/2023 12:25 PM | |
Joined: 3/9/2023 Last visit: 3/13/2023 Posts: 6 Rating: (0) |
Thanks ;) |
3/10/2023 1:47 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986) |
o you mean FileWriteC? |
3/10/2023 1:51 PM | |
Joined: 3/9/2023 Last visit: 3/13/2023 Posts: 6 Rating: (0) |
Yes,sorry. |
3/10/2023 1:52 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986) |
then the answer is no card no write no read this commands work only on the memorycard. |
Follow us on