7/6/2006 7:38 AM | |
Posts: 5 Rating:
|
How I can made a VPN connection with Hardware VPN Router, and whitch software I need on remote and office computer? How much it cost ? (approximatly) |
7/6/2006 11:19 AM | |
Joined: 8/31/2005 Last visit: 9/16/2025 Posts: 217 Rating:
|
Hi! Some more resources on VPN: |
Greetings, Chris |
|
7/7/2006 8:38 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="mate1320"]I have an PLC connected to the PC through ethernet card 1 and PC is conected to the internet via ADSL modem, through etherned card 2 . This PC is reachable through VPN line, from my office. I need to edit/monitor a program remotely from my office. My office PC is connected to internet too. What i have to do? Hi, The Scalance S612 is the device you are looking for.... [:o] See the handbook for this equipment in the next link: SCALANCE S602, SCALALANCE S612, SCALANCE S613 and SOFTNET Security Client Some more information about the S612: [;)] Product description SCALANCE S Security Modules are the core of the new pathbreaking industrial security concept by Siemens Automation & Drives, based on the protection of automation cells and network segments. This enables an even more effective protection of the automation network against danger from inside, such as deliberate or undeliberate incorrect accessing by employees and excessive or unnecessary communication load. In the case of remote accessing via unsafe networks, such as Internet or WAN, encryption can be used to safeguard the communication against data espionage and manipulation. As a result of the increasing integrated Ethernet-based interconnection of automation networks with other networks (e.g. MES or office networks), or connection to company Intranets and remote maintenance via WAN or Internet, modern industrial communication is subject to considerable risks and dangers. Existing security concepts designed for office environments are no longer sufficient for the special requirements of automation technology, because
Functions Security functions
Every incoming data stream is monitored and checked. In view of the fact that IP addresses can be forged (IP spoofing), checking the IP address (of the client access) is not enough. In addition, client PCs may have changing IP addresses. For this reason authentication is carried out by means of proven VPN mechanisms.
Safe encryption is needed to protect the data exchange against espionage and manipulation. In this way the data will remain unintelligable for any eavesdropper in the network. The Security Modulewill establish a VPN tunnel to other Security Modules for this purpose.
To be able to identify and follow-up attack or access attempts, such data can be stored in a log file and read out with the configuration tool.
The configuration can also be done by users posessing no deeper knowledge about security mechanisms.The minimum configuration needed is to allocate the Security Modules of a network to groups. Only the modules within a group can establish VPN tunnels with one another. This ensures that only safely authenticated and authorized devices can access a network subscriber protected by a Security Module. Above that the data transmission is encrypted and in this way protected against espionage and manipulation. In view of the fact that the configuration tool generates the VPN certificates, no elaborate PKI infrastructure or separate creation or loading of keys is necessary! Automatic learning by the subscribers of the internal network and recognizing of other Security Modules in a network ensures a minimum of configuration work and also enables dynamic expansion without much configuration! The configuration tool is included in the scope of supply of SCALANCE S.
The C-PLUG (Configuration Plug) is available as an option to save all the configuration data of a SCALANCE S module. If a SCALANCE S device should fail, the C-PLUG can be removed and plugged into the new SCALANCE S device, so that downtime is reduced considerably. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
7/11/2006 7:56 PM | |
Joined: 4/6/2006 Last visit: 6/24/2025 Posts: 604 Rating:
|
Dear all, Since a couple days there is a brand new FAQ available and since it has something to do with this topic, here is the link: What options exist for establishing a VPN tunnel with a SCALANCE S module S612/S613 via a public network (WAN)? I think that this information could be usefull. [8)] Best regards, INS |
Best regards, |
|
Follow us on