1/22/2020 10:12 AM | |
Joined: 1/6/2019 Last visit: 8/27/2022 Posts: 13 Rating:
|
Hi guys, attached all informations about my project i am using 2 CPU s7 410-5h with 443-1ex30-0xe1 v3.2 cps i am trying to test my program with modsim32 simulator port n° in simulator is 502 and ip adress of host pc is 192.168.0.20 always i have A0FF in status-0 and status-1 , sometimes when busy = 1 status_0 = A092 ( but LENGTH or START_ADDRESS are correct) i put use_all = 0 to send frame just with first connection ( same erroreven if use_all=1 ) i change UNIT= 0 , same error what should i do to ensure communication AttachmentA0FF.zip (331 Downloads) |
1/22/2020 12:13 PM | |
Joined: 1/6/2019 Last visit: 8/27/2022 Posts: 13 Rating:
|
Right now i am able to receive data but i am not finding data in DB 11!! Attachmentreceive.zip (293 Downloads) |
1/22/2020 12:37 PM | |
Joined: 10/3/2008 Last visit: 9/8/2025 Posts: 996 Rating:
|
I knew ModSim32 as a client, not as a server. But it seems, that is a server... Address 40001 is absolute modbus address 0, 40002 is absolute modbus address 1 and so on. 4000x are the address area in the application layer, but the modbus block don't use the application layer, but the absolute addresses.
|
Last edited by: Wüstenräuber at: 01/22/2020 12:39:26Last edited by: Wüstenräuber at: 02/04/2020 09:11:41Last edited by: Wüstenräuber at: 02/04/2020 09:13:41 |
|
Follow us on