11/25/2024 9:27 AM | |
Joined: 5/30/2022 Last visit: 9/12/2025 Posts: 634 Rating:
|
Hi Riyaz123, In the following application example I have not found reference to the UNIT_ID, which is used to communicate via Modbus through a gateway, so I do not know if such communication is possible, you may have to look at a S7-1200 that does have that option in the MB_CLIENT block: How do you implement MODBUS communication with S7-200? What is the function of the "MB_UNIT_ID" in the instance data block of the Modbus block "MB_CLIENT"? |
If this information really helps, you could use the Rate function. |
|
Follow us on