4/30/2014 11:54 AM | |
Joined: 2/10/2006 Last visit: 6/2/2025 Posts: 149 Rating:
|
Hi NavBi, Attached is a zipped folder with a program example for TI505 PLC. it comes originally from the Protool Pro V6.0 CD. It was built for OP25, OP35, OP37. To my knowledge the driver has not changed so i am guessing it will work for MP377 also. How to use is expalained in the readme.txt file. You will need Tisoft7 and Com Profibus V5.2. This is all quite old and obsolete. Alternativley you could use PLC Workshop for 505 from Fastrak Softworks which has a built in Profibus configurator. Hope this helps, Carlo AttachmentSIMATIC_505DP.zip (950 Downloads) |
This contribution was helpful to
1 thankful Users |
7/24/2014 4:23 PM | |
Posts: 4 Rating:
|
Hello Sam, Thanks for the help. With the Fap.REC file and project provided by you. I am not able to make the communication happen. From somewhere i got the HMIl.REC file and foundattached document. I followed the instruction mentioned in it and communication is working. But it is only working with middle model and not with tiny, small and big. Please help me with the following queries 1.Do we need to create HMI.REC / FAP.RECourself or we will get with some software. As it is not with WInCC flexible installation? 2. How to make the communication work with other model size like tiny, small and big? 3. What mistake i am making with FAP.REC as i am doing the same steps as done with HMI.REC but using the XSUBs in readme.txt file, it is written "You will need to add your xsub entry points to header.src." Do i need to do something if yes then what? Thanks AttachmentD:\TI505_Profibus_WinCCFlex_[1].pdf (1056 Downloads) |
Last edited by: NavBi at: 7/24/2014 4:23 PM |
|
Follow us on