2/13/2024 12:57 PM | |
Joined: 7/19/2022 Last visit: 6/3/2024 Posts: 361 Rating: (61) |
Hello Cvetozar Popov, You must follow the instructions in this FAQ: Monitoring Machines and Plants with Network Cameras and SIMATIC HMI Comfort Panels It is recommended to do it via RSTP. If it still gives you problems, I would recommend updating the panel to the latest version available. The integrated browser cannot be updated except with the panel's own updates. Also try an empty project where it only shows the camera in case it is a performance issue. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on