7/18/2012 9:17 AM | |
Posts: 3 Rating: (0) |
Yes, according to the requirements of the project, I shall be using radio telemetry only |
7/18/2012 4:01 PM | |
Posts: 378 Rating: (73) |
Hello kamish, I have done a project a little bit similar to yours radio communication but my the communication range is <1km. I have used VEGA's radio data transmission device with profibus interface to communicate between S7-200 and S7-300(master) PLC. Well as my understanding, your project is feasible, if your hardware's Modbus RTU speed meets your requirement. By the way can you tell me your device brand and model? Because I am impressed with it's long distance functionality. Regards, |
Follow us on