9/22/2014 6:50 PM | |
Joined: 10/24/2012 Last visit: 10/18/2024 Posts: 310 Rating:
|
Dear Experts, I am having trouble while fetching data of my S7-1200 in OPC Scout.I search on the internet and found a example https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=39960679&caller=view this is the link of that example,i made the same steps as provided in the manual,but i stuck at the last point.When i try to get data my connection doesnt show anything and i am unable to configure the variables manually.Because when i tried to configure them manually and give the ID but unable to find the SERVER.Kindly please help me.Attached is the screen shot of configuration editor and OPC scout. Thanks in advance. Attachment2.zip (302 Downloads) |
Kashir Saeed. |
|
This contribution was helpful to
1 thankful Users |
9/25/2014 6:59 PM | |
Joined: 10/24/2012 Last visit: 10/18/2024 Posts: 310 Rating:
|
Dear Fafner, How can i check the connection status? My OPC scout v10 doesn't show the option new connection in any of the field like M,I,Q,DB etc. Now i have done that with OPC SCOUT 2.5 Navigator.But a new problem arrises.Now i am able to connect everything excpet DB my DB shows a cross sign in OPC Navigator and OPC Scout V10 too. I can add the values manually to the DA View of OPC SCOUT V10 but that is not my concern.I am using WINCC to fetch the tags from PLC and to show it in DCS room.Now anyone can tell me how to add a DB in OPC.I am using S7-1214 DC/DC/DC.Attached is the screen shots of the OPC. Thanks in advance.
AttachmentDB_Cross.zip (173 Downloads) |
Kashir Saeed. |
|
9/25/2014 10:52 PM | |
Joined: 9/3/2008 Last visit: 10/11/2024 Posts: 928 Rating:
|
Kashir, I suspect it is an issue with the setup of the PC Station/OPC server in the Step7 project. Try to have a look at the last 3 messages in this thread: /tf/WW/en/Posts/114250#top |
Michael |
|
This contribution was helpful to
1 thankful Users |
9/28/2014 9:24 AM | |
Joined: 10/24/2012 Last visit: 10/18/2024 Posts: 310 Rating:
|
Dear Michael as i read in the forum its not the issue of PCstation or OPC server actually its the problem with S7-1200 anyhow i read the DB by adding it manually in my DA view.
|
Kashir Saeed. |
|
Follow us on