8/11/2020 8:34 PM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
Hi my question is Here in program %L18.0 is being used But in the temp the last variable is Power State which is integer so it will occupy byte 16 and byte 17 so basically 18 is not allocated to any variable so is it okay to use address %L18.0 ------------------------------------------------------------------------------------------ |
Last edited by: qwemx at: 08/11/2020 21:26:19Last edited by: Jen_Moderator at: 08/12/2020 11:09:07New subject after splitting With kind regards... |
|
8/12/2020 8:16 AM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
I believe this is converted code and was not written in STL originally. |
With kind regards... |
|
8/12/2020 9:37 AM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
I want it to be in Ladder or SCL but not in STL I have another library from s7-1500 which in Ladder but when compiled in S7-300 it has some errors AttachmentABB LIBRARY FOR 1500.pdf (51 Downloads) |
With kind regards... |
|
8/12/2020 9:58 AM | |
Joined: 12/18/2014 Last visit: 5/23/2024 Posts: 33100 Rating: (4085) |
And what does it all have to do with the local data that this topic is actually about? |
Follow us on