4/26/2018 11:02 AM | |
Joined: 2/20/2018 Last visit: 5/27/2024 Posts: 46 Rating: (0) |
I would like to answer also about the breakpoints settings. I have very strange situation in my project. I can set the breakpoints on almost every functions except one. The functions has been written in STL. Of course I remember that I should disable googles (monitor online), go to ONLINE mode and turn on the "test operation" from the Debug > Operation... options. Everything will be ok but I can not set any breakpoints only in one of the STL project function FCxx. What can be the reason of this situatiuon, please help! PS. I am sure that no compilation errors in my project... PS. This function has inside many pointers reference... I have no idea what is the reason of this unnormal situation, please help me. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/26/2018 11:48:11 AMNew subject after splitting Adam |
|
4/26/2018 4:10 PM | |
Joined: 10/25/2016 Last visit: 9/1/2022 Posts: 199 Rating: (25) |
Hi, Breakpoints are available only in STL, Sometimes you see STL language on the screen however the language has been set on LAD or FBD... so make sure you are in STL (View Tab, and Select STL) Regards |
Follow us on