6/14/2024 12:16 PM | |
Joined: 5/28/2018 Last visit: 6/14/2024 Posts: 85 Rating: (4) |
Hello, Is there a way to change IP address of PLC by the program? Thanks |
6/14/2024 1:02 PM | |
Joined: 3/11/2019 Last visit: 6/20/2024 Posts: 1477 Rating: (266)
|
Hi, you can have a look at instruction T_CONFIG. How do you configure the Ethernet interface of a CP/CM program-controlled with T_CONFIG in TIA Portal?The "T_CONFIG" instruction is used for program-controlled configuration of the integrated PROFINET interfaces of the CPU or the Ethernet interface of a CP/CM. You can use T_CONFIG to change parameters such as the IP address in TIA Portal during operation. Description T_CONFIGProgram example for T_CONFIGregards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on