9/16/2010 4:46 PM | |
Posts: 8 Rating:
|
hello Denilson ... I write to you from South Africa ... Johannesburg ... I have found and downloaded your program - for ... serial.zip .... and also ... HyperTerminalReceive_RS232 ... I am surprised at how simple it really is.... I am sure though that you need to use the other faculties of the PtP system, for serial..???? yes..??? - or NO..??? Unfortunately - I do not have the serial port for my 1212C - S7-1200..... but nevertheless - it is good to try to learn something newer everyday...!!!!!! [schnippschnapp] 2) - I would like to make a project - where I have three (3) counters, or more- (UP Count) - so they are daisy chained.... I have that worked out I think... so that units counter is ...1 .... and then 10's counter is to 10 .... and then hundreds counter is to 100's ....etc.. (the wish - is to count some pulses from a "power unit" - that gives 1 pulse for every 100 watt power used.. then I wish to count these pulses - and then SEND them from the CV value for the counters - on the serial port ...to my PC = which has a program - to write RS232 incoming values to a file...).. so I need to read CV(1) - and send data ... switch to CV(10) and send data value... and then switch to CV(100)... read data - and send to PC... on serial port... (of course - I have only three counters - but the wish is to have maybe 1's...10's...100's...1000's ..... 10000's - so that I can count like in power meter mode...hmmm.. How do I write / draw the LAD file, so that I can do this..... please..??? Excuse me for wanting to fly before I can even crawl... but that is me..!!!!... With this method - I can keep software overheads cheap.... and can save the data - in simple text format - in file on the PC, for present performance - and history performance of said energy pattern / usage levels...hmmm.. Denilson - I thank you very much - you are an inspiration.... to me... My Kindest Regards Spencer Sabatta Johannesburg South Africa.. Splitted from Sample program S7-1200 RS 232 ASCII HypterTerminal comunications. |
Last edited by: O_Moderator at: 9/20/2010 12:31 PMLast edited by: O_Moderator at: 9/20/2010 12:28 PMnew subject after splitting |
|
Follow us on