8/17/2009 5:34 AM | |
Posts: 14 Rating: (1) |
Is there a finction block in Step7 to directly convert DateTime data format to integers. If not, does anyone have sample code for this function. Thanks, Kris |
8/17/2009 5:17 PM | |
Posts: 88 Rating: (0) |
Which software do you want to use ? STL or SCL ? with SCL, you can take information from SCL online help.. (converisiton function) |
8/20/2009 1:47 PM | |
Posts: 49 Rating: (1) |
DEAR CHOPPER SEE ATTACHED FILE IF IT CAN HELP YOU IT IS A CODE TO EXTRACT DATE AND TIME SEPERATELY FROM DATE AND TIME DATATYPE EXPLAINED IN SIMATIC MANAGER HELP AttachmentDATE AND TIME FUNCTION.zip (270 Downloads) |
This contribution was helpful to1 thankful Users |
8/20/2009 8:10 PM | |
Joined: 10/23/2005 Last visit: 3/31/2020 Posts: 81 Rating: (9) |
Chopper, Here is how I have done it and it has worked fine for me. I did it in LAD because there wasn't BCD conversion in SCL when I started. The first page there is another ladder for the seconds. You just have to rin this block in OB1 to get Date and Time from there. Dont worry about the time snyc inputs. This block also had a time sync where it would update the date time from another device that could write to it. So all you need in the #OB1_Date_Time for an input and your outputs. Good Luck AttachmentConvert Date and time to ints.pdf (364 Downloads) |
9/4/2009 12:34 PM | |
Posts: 9 Rating: (2) |
Hi, I hope my functions can help you. Ciao AttachmentRead - Set CLOCK PLC - INTEGER format.zip (213 Downloads) |
This contribution was helpful to1 thankful Users |
9/4/2009 4:08 PM | |
Posts: 4 Rating: (2) |
Please find the solution I used in the attached project file. This converts system time to integers and is done in ladder. Hope this helps someone. Thanks to all for the help. Kris AttachmentS7_tim~1.zip (262 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on