6/20/2022 1:52 PM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating:
|
Drives - quick commissioning with STARTER (Check out this for your quick reference for Drive Selection In Starter)
|
Last edited by: Jen_Moderator at: 06/21/2022 07:14:23Video embedded. If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
6/21/2022 9:20 AM | |
Joined: 9/30/2016 Last visit: 6/12/2024 Posts: 913 Rating:
|
Thank you for answering Jack, My situation is however different: I do not want to use the wizard and make a potentially different set of parameters. I have a machine - with 4 similar drives (and one of a different type) where the CU has become defective on the 3. rd drive. I want to switch the defective CU with a new one and download the parameters that I have in my project (from our backup system) and run again with the same parameters as before the CU became defective. In THAT case - how do I search for the replaced CU card from within my project (that already has the parameters)?
|
Follow us on