7/14/2021 2:45 PM | |
Joined: 9/12/2020 Last visit: 4/29/2022 Posts: 23 Rating: (0) |
HI Please advice me how to create a new post for the new topic in this forum. I do not understand it properly. I have a question about disk type tool magazine. 1. How I will use M06 command DB2500.DBX111.6 in ladder. I have not find it in a default ladder of 808D advanced controller. Instead I have found M21 and M22. 2. When a disk magazine is ready to change tool , Which M command is required to change the pocket position from horizontal to tool change position and arm movement to finish the cycle. I am little bit confused. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/15/2021 07:50:43New subject after splitting |
|
7/15/2021 6:35 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (874)
|
Open product conference e.g. SINUMERIK CNC automation systems, on top center you will find Actions, Legend , Experts & New topic keys. Click on New topic key which will open new topic wherein you may post your query.
M6 is auxiliary function call which calls tool change sub-program & need not to be used in PLC. Please refer attached sheet which expalins tool change program & machine data settings.
In tool change or tool management, user need to call an appropriate tool number & not M or pocket position. In tool turret , define tool type & tool offset data in relation to location number (turret tool holder number) so that as per machining operation requirement, related tool number is call. HTH |
This contribution was helpful to1 thankful Users |
7/16/2021 5:18 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (874)
|
T02 will call tool number 2 & m6 will intiate tool change cycle.
DB2500.DBD2000 is tool type & offset DINT data type & inetrnally read in tool change cycle.
Please refer SINUMERIK 808D ADVANCED Commissioning Manual |
Last edited by: Jen_Moderator at: 07/16/2021 06:08:19Optimized link. |
|
7/16/2021 1:54 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (874)
|
SINUMERIK 808D ADVANCED Commissioning Manual
It comes along with Tool box CD |
Follow us on