2/22/2009 9:59 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, Be aware that M4.1 is a bit of MB4, but also a bit from MW4 (=MB4+MB5), or MW3 (= MB3+MB4), ... So, when making a cross reference, look also to these. For basics of programming look to this: Statement List (STL) for S7-300 and S7-400 Programming http://support.automation.siemens.com/WW/view/en/18653496 Ladder Logic (LAD) for S7-300 and S7-400 Programming http://support.automation.siemens.com/WW/view/en/18654395 Function Block Diagram (FBD) for S7-300 and S7-400 Programming http://support.automation.siemens.com/WW/view/en/18652644 |
Best regards |
|
This contribution was helpful to1 thankful Users |
2/23/2009 9:25 PM | |
Posts: 15 Rating: (0) |
@Ayman Elotaify You havent posted a screenshow. So, to summarize, if I cant find any byte, word or double word that contains this bit, then its of no use? @Sidney Thanks for the info. Why would then somone want to use peripheral addressing instead of using process image table? |
2/28/2009 10:01 AM | |
Posts: 15 Rating: (0) |
Thanks, Sydney. |
Follow us on