3/26/2014 9:13 AM | |
Joined: 10/7/2005 Last visit: 6/7/2024 Posts: 3008 Rating: (1051)
|
Hello AUS_MB
Ussage of a global DB as an additional call up path criteria will work with FC's just as well as with FB's (with FB's you can additionally or exclusively nonimate thespecific instance DB). That is possible too, but in this case easiest done directly via right click on the specific FC from within the calling Block and item 8 of the above link has the details on this. I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
8/31/2018 12:25 PM | |
Joined: 11/7/2011 Last visit: 1/27/2023 Posts: 96 Rating: (0) |
IN CASE OF FC'S ,IF MORE THAN ONE DB IS USED ,THEN IS IT POSSIBLE TO MONITOR. |
Follow us on