3/7/2013 5:42 PM | |
Posts: 4 Rating: (0) |
Hello, We haven't made any soft or hardware changes. I uploaded this FC272 that is called on OB1 and makes a call to the FB161 that I'm having problems (i will uploaded in the next post). Thank you. Alcídio
AttachmentFC272.pdf (41 Downloads) |
3/8/2013 12:22 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Hello, Comparison of blocks are possible.See the attachment as I have done it for 2 FCs in a project.I copy FC1 and rename it as FC2 .Then changed some codes inside and also add new interface as input to FC2. You can see the result.All parameters are different.You can find "measmon" in PCS7 libraries and compare it with what you have in your project. Best regards Hamid Hosseini Attachmentcompare.zip (25 Downloads) |
Follow us on