10/31/2018 11:21 AM | |
Joined: 9/21/2012 Last visit: 4/28/2024 Posts: 3931 Rating: (444) |
The same MLFB number can have different versions, so you need to precise when you select the module from HW catalog. You can get the latest updates by updating the HW catalogue through HW configuration (Options -> Install HW Updates -> download from internet -> Excecute). If your PN/PN coupler is the latest PN/PN coupler v4.0, you need to download the GSD for it. To configure the actual communication, i would use a bigger data area than you actually need. This just if you need to move more data, you don't need to do any changes to the hardware configuration. Now you need 3 bytes, but i would configure 10 bytes at least. I Personally prefer to use: Universal module (allocates inputs and outptus). It's not so sensitive for configuring the IN an OUT in the correct order on both sides of the communication. If you have the PN/PN coupler physically in your end, use X1. To the other end configure X2. |
Last edited by: Hati at: 10/31/2018 11:22:03 AMLast edited by: Jen_Moderator at: 10/31/2018 2:10:52 PMOptimized link. |
|
Follow us on