6/4/2015 8:30 AM | |
Joined: 12/13/2013 Last visit: 4/5/2024 Posts: 36 Rating: (0) |
Sir, I am trying to do power failure retraction in 828D System having system software 4.4 on the Lathe Machine. Have tries the retraction with the ASUP method. Details of the methods are been attached. Find the observations as belowwhich are tried in MDA Mode: 1) If only Spindle (Chuck) rotating then retraction is working till the specified distance. 2) If only Z Axis is moving then retraction is working till the specified distance. 3) If both Z Axis & Spindle(Chuck) are moving the retraction behavior is eratic i.e. sometimes it is not happening or if it works then only 0.6mm max movement is happening. This retraction is required as the customer requires during threading operations with the specified retraction distance. Kindly Help guide me to resolve this problem. Regards, Rohit Jage AttachmentEmergency_retraction_SINUMERIK 828D.pdf (176 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on