8/20/2015 11:16 AM | |
Joined: 8/26/2009 Last visit: 4/12/2024 Posts: 41 Rating: (2) |
Well, I am extremely surprised that no one ever in this forum came across this issue. |
8/20/2015 3:26 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Dear User, The easiest way would be using "Report System Error" in HW.Config . If you assign an FB/DB in user block tab, then some extra information would be available for you.The most important ones would be logic address, error number and some others.For error number, you can access an explanation that list is available to export in general tab.I think it is easy to send a WORD to a DCS with explanation for each possible number. The other way, a bit difficult, to find out all errors by yourself.You need to check and select OBs/SFCs based on your modules used.The following manual would be a great help for you: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 Good Luck, hdhosseini |
Last edited by: hdhosseini at: 8/24/2015 5:29:02 PM |
|
6/6/2017 8:28 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Tolis, U can use SSL-ID W#16#0C91. INDEX · For the partial list extract with SSL-ID W#16#0C91:· S7-400: bits 0 to 14: logical base address of the module Bit 15: 0 = input, 1 = output· S7-300: bits 0 to 14: any logical base address of the module Bit 15: 0 = input, 1 = output. Also for report system errors, u should assign names to all the modules to distinguish it from from one another. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
6/6/2017 12:33 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Tolis, Have a look at the manual-- https://support.industry.siemens.com/cs/ww/en/view/54757136 You can call SFC51[SSL-ID: W#16#00B1] or 59 in OB82 in the user program to view detailed diagnostics data output by the module. Have a try with SFC59 also. |
Last edited by: Min_Moderator at: 6/9/2017 3:47:02 PMReplace link If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on