8/15/2022 7:57 AM | |
Joined: 5/12/2006 Last visit: 6/14/2024 Posts: 22263 Rating: (2989) |
is the adapter detected in the Device manager? Which order number have the adapter? |
8/15/2022 10:34 AM | |
Joined: 4/6/2021 Last visit: 5/24/2024 Posts: 21 Rating: (0) |
yes.it is detecting We have 6GK1571-0BA00-0AA0 adapter |
10/13/2022 7:33 AM | |
Joined: 4/6/2021 Last visit: 5/24/2024 Posts: 21 Rating: (0) |
In attached selection communication become ok |
10/13/2022 8:11 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Yes it is OK & detected also. Click on accept button. |
Follow us on