10/2/2016 11:23 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello, Have you already seen this: https://support.industry.siemens.com/tf/ww/en/posts/screen-shot-export/92986/? https://support.industry.siemens.com/cs/document/109562021/export-graphics-tool%3A-for-exporting-graphics-from-wincc-(tia-portal)-to-a-local-directory-as-original-file-type?lc=en-WW |
10/2/2016 11:50 AM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following topic: How do you create screenshots of configured HMI screens with WinCC (TIA Portal)? |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to4 thankful Users |
12/2/2019 5:29 PM | |
Joined: 3/1/2019 Last visit: 6/13/2024 Posts: 17 Rating: (0) |
Hi, I used your suggestion but my screen got undersized. Any word? |
9/30/2020 1:16 PM | |
Joined: 3/10/2020 Last visit: 5/17/2023 Posts: 27 Rating: (0) |
This is brutal printing method. Takes forever and prints all details of each object on the screen in tables |
9/30/2020 3:28 PM | |
Joined: 7/7/2010 Last visit: 6/17/2024 Posts: 14808 Rating: (2381)
|
There are software applications well suited to screen grabs from the active window with a repeatable start x/y and stop x/y "pixel" location, which an HMI screen grab would certainly qualify for, if all screens were configured for 100% (or at least the same) zoom levels. You can find them in the screen scrapers category of software tools via online searches. In this way, you can quickly navigate through all the screens, use a hot-key combination to cause the screen scraping, and with a little bit of thought, automatically name the screen captures in order of screen grabs. I use such a thing for home automation data, collecting snippets of data, presenting onto a dashboard of sorts.
|
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on