1/13/2015 4:30 PM | |
Posts: 18 Rating:
|
I have also an error := Look attachment, You can see that my service packs are availible for every product in the error message. I've repaired all the products two times but still the error. It's strange that TIA says all packages are SP1 but my control panel says V13 (see picture) Does anybody know what to do and help me? Thanks ---------- New subject after splitting from Error installing TiaPortal V13. |
Last edited by: Min_Moderator at: 1/13/2015 4:44 PMSplitted |
|
1/13/2015 4:40 PM | |
Posts: 18 Rating:
|
But that dvd is not published yet....... or can i take the V13? |
1/13/2015 5:13 PM | |
Joined: 5/12/2006 Last visit: 7/8/2024 Posts: 22299 Rating:
|
Hello, no you can't take the V13, that's the installation which you have already installed ;) here you can download the DVD which includes the TIA Openness V13.0 SP1 Regards Christoph |
Last edited by: ChristophD at: 1/13/2015 5:38 PM |
|
This contribution was helpful to
1 thankful Users |
1/14/2015 8:04 AM | |
Posts: 18 Rating:
|
Thanks But it's still a shame it doesn't install automatic with the rest of the STEP 7 professional. |
Follow us on