8/23/2011 1:12 PM | |
Joined: 10/3/2010 Last visit: 5/29/2024 Posts: 1552 Rating: (188) |
Is there a way to write an alternative in C-scipting for the "Left", "Mid" & "Right" VBS-functions? I need to adjust existing C-scripts and I need to extract the last 5 characters of existing strings with a fixed length? For example each strings contains 15 characters and I need to check the last 5 characters only. Thanks in advance. |
B r g d s , |
|
8/23/2011 2:20 PM | |
Posts: 1776 Rating: (95)
|
Hi, see FAQs http://support.automation.siemens.com/WW/view/en/26728674 |
This contribution was helpful to1 thankful Users |
8/23/2011 2:40 PM | |
Joined: 10/3/2010 Last visit: 5/29/2024 Posts: 1552 Rating: (188) |
Thanks April , that looks quite interesting. I'm not a C-script expert, so can you point me in the right direction for creating a "Right"-function. Can't see it in those FAQ at first quick look |
B r g d s , |
|
9/22/2011 9:19 AM | |
Joined: 10/3/2010 Last visit: 5/29/2024 Posts: 1552 Rating: (188) |
Perhaps an example in c-script to achieve to following: if you have in a script a string "Not_needed_now" and you want to reduce this to "needed_now", how can you do this in c? In VBS, it's much easier but I can't use VBS in this project. thanks |
B r g d s , |
|
Follow us on