9/30/2019 10:33 AM | |
Joined: 3/20/2017 Last visit: 1/14/2021 Posts: 10 Rating: (0) |
Hi All, I want to backup HMI File on SIJECT OP 37(OEM OP37 Novapak). I use the cable that I usually use to download HMI File to OP 270, MP 270 and works well with these 2 HMI panel.. I already setting the port setup on my laptop and prosave(picture attached), also make SIJECT OP 37 go to transfer mode(picture attached). I use USB to Serial Converter in order to connect the cable to my laptop. I connect my cable to Port IF2(Config. / Printer Interface) on the HMI Panel. The result was fail to connect to HMI Panel.
Cable connection from 15 pin Sub D and 9 pin Sub D which I make myself is also attahed. Is there some settings that i missed in order to successful connect to this SIJECT OP 37 HMI Panel? Thank you All Michael Jie AttachmentImages.zip (92 Downloads) |
Follow us on