9/1/2023 2:31 PM | |
Joined: 7/10/2021 Last visit: 9/1/2023 Posts: 2 Rating:
|
I am currently using an S7 1513-1pn plc in Tia Portal conected with 6ra80000MV620AA0 profibus communication. From simotion scout I am using telegram 999 and have the control unit switching on and off with no errors. For some reason however, I cannot get the DC motor to turn. Looking at the control panel in SIMOTION SCOUT it shows all neccesary bits are set apart from "Setpoint enable" bit in the control word and am assuming this is the problem. enable operation bit not high when i set cmd with plc whats control panel assume . Can this bit be forced in SCOUT or is it set within the telegram? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2023 12:21:55New subject after splitting |
|
Follow us on