9/3/2013 3:40 PM | |
Joined: 7/7/2010 Last visit: 9/17/2024 Posts: 15193 Rating: (2417)
|
Part 1 above: the documentation for the s7-300 PLC states the programming package is STEP 7 V5.3 SP1. Contact Support Requestto see if there is a TIA Portal hardware support pack that includes that plc. Part 2 above: the 3rd party GSD will not show up in the Siemens hardware devices portion of the catalog (unless the 3rd party is Siemens). Look in the device tree, likely towards the bottom of the list for "other" devices. Expand the tree until the device appears. It is possible the portal and the gsd are incompatible, in which case, you would need to contact the vendor for support. They may have a FAQ on how to integrate their hardware into the Portal software. Have you checked with them? |
science guy |
|
This contribution was helpful to1 thankful Users |
Follow us on