12/23/2016 11:07 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi BALAKRISHNAN92, User is not permitted to program these blocks or even interconnect. These are generated & interconnected automatically when 'Generate module drivers' is on. However note- S7 F - ET 200S Fail-Safe Modules S7 F - ET 200pro Fail-Safe Modules S7 F - Safety Engineering in SIMATIC S7 S7 F - S7-300/ET 200M Fail-Safe Signal Modules S7 F - ET 200eco Fail-Safe IO Module S7 F - ET 200iSP, Fail-Safe Modules So SM326 is failsafe IO. |
Last edited by: Sachinpatke at: 12/23/2016 6:17:32 PMIf you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
Follow us on