10/2/2020 9:40 AM | |
Joined: 11/15/2018 Last visit: 12/30/2021 Posts: 8 Rating: (0) |
Hello everyone, I have similar problem. My task was to modify HMI Panel MP 377 12" Touch to add few extra buttons regarding the operation machine. The communication was running good previously. But as soon as I modified the programm and load into the HMI, the communication has been brokern and could not estabilish back even by loading backup programm. I have confirmed the IP addresses of both SIMOTION and HMI (172.19.1.39 and 172.19.1.40). It would be grateful if someone helps me in this regard. Thanks Anil ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/02/2020 12:10:51New subject after splitting |
|
10/2/2020 12:15 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
Closed cause question posted twice. The second thread with the subject Communication problem between SIMOTION and HMI Panel MP377 12" Touch is published within the conference SIMATIC Panel. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on