10/24/2023 10:44 AM | |
Joined: 3/7/2023 Last visit: 7/4/2024 Posts: 17 Rating: (0) |
Can anyone suggest how to do the programming for TMPOSINPUT-1 (ET 200SP, TM Posinput 1 6ES7138-6BA01-0BA0) using S7 1200 PLC. We are replacing the Existing S5 High speed counter module 6ES5 385-8MB11 25/500KHZ.instead of this module we are using the TM posinput 1.but in the programming and wiring part we want to know how to do and there is already existing program is there it should be STL .we cant convert it so we need to do the programming for this . Please suggest how to do. i have the Pin assignment of the existing High speed counter . Pin5- Ground Pin8-Supply voltage (24V) pin13-Rectang-wave signal A(24V) Pin14-Rectang-wave signal B(24V) we have only this information. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/24/2023 11:59:09New subject after splitting |
|
10/24/2023 12:02 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Need help to convert STL to Ladder is published within the conference STEP 7 (TIA Portal). Jen_Moderator |
10/25/2023 4:07 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by AutoGen_2655561 is split to a separate thread with the subject How to make the wiring between TMPOSINPUT-1 and S7 1200 PLC?. Best regards |
Follow us on