10/27/2020 9:11 PM | |
Joined: 1/21/2016 Last visit: 4/7/2024 Posts: 17 Rating:
|
Dear Wizard I have another TP900. I want to change its users and passwords. I made a complete backup from HMI. Then I made a new project with new users and passwords according your recommendation. But, when I want to download project to HMI, TIA asks me to update operating system due to difference between versions. The version of HMI is v11.00.02.04 (the attached figure). But I have TIA V15 which does not have this version (the lowest version is V12). If I update operating system, is it possible to transfer prosave backup to HMI again? We have DCS system, HMI is connected to CPU 313C-2DP through Profibus, then they are networked with CPU 414-5H. Updating can affect the other parts of system? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/28/2020 08:58:45New subject after splitting |
|
10/27/2020 9:33 PM | |
Joined: 3/30/2020 Last visit: 6/28/2024 Posts: 4623 Rating:
|
Do you have the option to NOT upgrade? I am guessing it is possible to proceed without doing an upgrade. All HMI images can be found here: Images that are not part of the original installation should be available on the mentioned web page. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/28/2020 5:05 PM | |
Joined: 1/21/2016 Last visit: 4/7/2024 Posts: 17 Rating:
|
|
Follow us on