2/11/2015 3:51 PM | |
Joined: 12/7/2011 Last visit: 8/16/2024 Posts: 384 Rating: (9) |
Hi Georg, Unfortunately i've another problem with the IIS configuration. When open the IIS (6.0) management i try to connect with the host, and i receive this error: "Impossible to connect at the local host. In the destination server is not installed the SMTP service. Is not possible manage a WEB or FTP server IIS7.5 using IIS 6.0" I try to installed the IIS 7.5 but i don't know if this is the right way. Any suggestion? Regards Alfredo ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/6/2017 1:19:04 PMNew subject after splitting |
|
2/13/2015 8:39 AM | |
Joined: 12/7/2011 Last visit: 8/16/2024 Posts: 384 Rating: (9) |
Good morning Georg, sorry for my delay, my currently situation is: if i open IIS from control panel, administration tool, i should see the connection with the local host. instead if i open the IIS from management computer, i see the SMTP service, but cannot browse the site. I have two dubt: 1) i'm connected with a wireless connection. 2) I've installed the web navigator by hand, i read that the web navigator should be installed before the SQL, and i don't do it. Do you think those point should be cause of my problem? Regard Alfredo. AttachmentIIS.pdf (216 Downloads) |
11/4/2017 7:53 AM | |
Joined: 11/3/2017 Last visit: 6/18/2024 Posts: 3 Rating: (0) |
hi , i am krishna. iam the new one for this. Is anybody can give me a hint about '' Web Navigator'' ? |
Follow us on