2/25/2007 9:40 AM | |
Posts: 71 Rating: (2) |
Hellow everyone I wanna know the frequency of the inputs " the minimum time bet. two successfull inputs " thanks |
2/25/2007 6:28 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
Hi Audy, That is not that easy to say, a Input have some time to switch to the internal electronics, the fastest input need 0,3mS there. After that the input have to be transported over the backplain where the input is on and after that it have to be transported over a network or is directly read in in the CPU. So there is a lot of timing, see the handbook: 15218045 Isochrone Mode 2006-03, you may also look in the handbook for example of the ET 200S where the timing is shown well. 1144348 ET 200S Distributed IO System 2006-10on D-1 the timing of the different IM 151 is shown. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on